SOLUTION
Marzoli provided Troung Phu Spinning with a complete spinning plant with 39,168 spindles that was assembled and installed at the beginning of 2023.
The project included:
- 2 complete Marzoli blow room lines which allows to process 1,000 kg/h of cotton. For 100% cotton an blend line whit weighting Bale
- 18 C701 cards
- 16 DF2 draw frames, double delivery
- 8 DFR1 draw frames, single delivery five of which equipped with autolevelr
- 1 LW3 Lap winder
- 6 CM7 combing machine.
- 6 FT6D roving frames with 240 spindles Double draft
- 24 MDS1 spinning frames, all equipped with:
- Marzoli slubbing device
- Marzoli compact device MAC 3000
Marzoli’s digital solution
To satisfy its needs for excellence, Troung Phu Spinning has relied on Marzoli’s digital solution: Marzoli YarNet allows to easily control and manage the entire spinning process as well as every single machine from your computer.
RESULTS
Currently the total production capacity of Troung Phu Spinning is of 23 tons/ month of yarn. TRUONG PHU SPINNING s also able to assure outstanding quality, that represents its main strength.
“Marzoli, has greatly contributed to the outstanding results that we have achieved, not only for the excellent technological level of its machines, but also by proving to be a competent and reliable partner”