Certifications

Operating with the purpose of “Total Quality” means also being able to confirm our commitment through the achievement of international certifications.

Operating with the purpose of “Total Quality” means also being able to confirm our commitment through the achievement of international certifications.

ISO 9001:2015

ISO 9001 certification represents both a guarantee for all our customers and a tool inside our company to constantly monitor the respect and effectiveness of the procedures.
Marzoli obtained from "Det Norske Veritas" the certification of the Quality System according to ISO 9001:2015.

 

ISO 14001:2015

ISO 14001 certification represents for Marzoli a fundamental tool to manage, in a structured and responsible way, the environmental aspects related to its activities, as well as a guarantee of commitment to sustainability for customers and stakeholders.
Marzoli has obtained Environmental Management System certification in accordance with UNI EN ISO 14001:2015, confirming its constant focus on reducing environmental impact and on the continuous improvement of its processes.

 

Green Label

The reduction of operating costs, as a positive effect of the application of sustainable technology, is an essential theme for the textile companies willing to compete successfully.
This awareness has fostered Marzoli to implement a process of continuous improvement, based on monitoring of the machinery performances and the adoption of carefully selected technologies and materials. This process has granted a constant reduction of energy consumption for all Marzoli machines, whose energetic performances are certified by the ACIMIT Green Label.
The ACIMIT green label is a document that identifies the energetic and environmental performances of textile machinery and makes them easily recognizable, using a process designated by the manufacturer as an evaluation parameter. The information reported on the Green Label is verified by an international certification organism, Rina, that guarantees the information authenticity.
 

Digital Ready

Digital Ready data model aims to standardize management and production data of Italian textile machinerybased on a common language that allows for easier integration of machinery within the manufacturing customer’s production systems.
The certification is designed to simplify the production process, making use of a standard language and unique data reading system that allows different types of machinery to dialogue with production systems.

Thanks to Digital ready customers benefits from:

  • Machinery ready to be integrated in production systems.
  • Reduction of production costs and times
  • Vision of the product’s entire lifecycle thanks to integrated machinery
  • Efficient overview of data with an easy-to-use dashboard
  • Simplified business analyses

Digital Ready is conceived by ACIMIT and specifically dedicated to Italian textile machinery manufacturers. The information reported on this certification are verified by an international certification organism, Rina, that guarantees the information authenticity.

See more